This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Can PRU-ICSS PWM with Phase Shift Operate at 96 kHz?

Part Number: AM2434

I have a question about the PRUICSS PWM sample.
Sample: PRU-ICSS PWM WITH PHASE SHIFT
Under the following conditions, I would like to operate with a carrier frequency of 96 kHz.
Is this possible? (By changing "PWM_OUTPUT_FREQ" in the code to 96000 and outputting the PWM waveform.)
If not, how high can the frequency be increased, and what is the limiting factor?

Conditions
  • Output 3-phase gate signals:
    UP/UN, VP/VN, WP/WN (3 pairs). Each pair should be complementary outputs.
  • Target motor: single axis.
  • Carrier frequency and dead time will not change during operation.
  • Duty cycle will change during operation.