Part Number: MSPM0L1306
Hello Experts,
We are starting to integrate MSPM0L1306SRTRR in a new product.
We like to use ROM-based BSL for first time flashing our application into MSPM0L1306SRTRR,
after this we want to fully disable the ROM based BSL.
I have 3 questions :
a) We only have TxD / RxD externally available. PA18 and NRST would be a big problem for us.
If the MCU is empty, does the MCU start automatically inside BSL ?
Or can we bring the MCU by command byte 0x22 into BSL ( if we cannot control PA18 / NRST ) ?
b) Can we use PA18 as free GPIO ? Or do we have to mind anything regarding PA18 to get into BSL for
loading our application one time into MCU and after this disabling the ROM based BSL ?
c) We want to control ROM based BSL by our test system. Can you send us the UART command set of
it ? Or is there any Windows DLL available ?
Thank you
Martin Rohrbach