This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010265: Compilation Errors After Importing TIDA-010265 Project

Part Number: TIDA-010265

Hello,

I recently imported the TIDA-010265 reference design project into Code Composer Studio. I have not made any changes to the code, but when I try to build the project I receive several compilation errors.

 

In addition, many source files and header files in the Project Explorer are marked as Excluded. 

Could you please advise on:

  1. Why several files are automatically excluded from the build after importing the TIDA-010265 project?

  2. How to correctly re-enable the necessary files or restore the original build configuration?

  3. Whether there is a specific CCS version or compiler version required for this reference design.

I have attached the screenshot of the errors and the excluded files for reference.

image.png

image.png

 

Thank you.

  • Hi Sathyen

    It is normal for driverlib folder and filed excluded in the project, because they replaced by driverlib.lib which already in the project. You do not need to modify anything, and do not required special version for CCS or Complier. And the warning message in your side are not error, you could go ahead debugging