Part Number: TIDM-02013
We need the Eval Sample Boards with the foloowing specification.
Input: Three Phave 380 V-415 AC
Output: 650 to 800 V DC
PFC :Active/Vienna
Output Power: 5kW /7KW/10kW
any standard eval boards are available to purchase?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDM-02013
We need the Eval Sample Boards with the foloowing specification.
Input: Three Phave 380 V-415 AC
Output: 650 to 800 V DC
PFC :Active/Vienna
Output Power: 5kW /7KW/10kW
any standard eval boards are available to purchase?
Hello,
This expert is currently out of office until next week. Please allow some time before they are back in order to formulate a response.
Best Regards,
Allison
Have you taken a look at TIDM1000?
Regards,
Chen