Hi,
We are currently evaluating a possible device replacement within the TM4C129x family and would like to confirm several technical points with TI.
-
Are TM4C1294KCPDTI and TM4C1294NCPDTI fully pin-compatible in the 128-pin TQFP package, including all GPIO alternate functions?
-
Are TM4C1294KCPDTI and TM4C129EKCPDTI / TM4C129ENCPDTI also pin-compatible with the same digital and peripheral function assignments, allowing drop-in replacement with no PCB modification?
Our understanding is that the crypto acceleration blocks (AES, DES, SHA, MD5) are internal modules and do not require additional external pins. -
If there are any differences in peripheral or digital function assignments between the TM4C1294 family and the TM4C129E family, could you please specify which pins differ?
-
Regarding HTTPS/TLS communication:
When switching from software-based cryptography to the hardware crypto engine, can we expect a significant performance improvement?
Since TI documents do not provide explicit speed comparisons, we would appreciate your guidance on the expected benefit.
Thank you very much for your support.
Conor