This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263PX-RESTRICTED-SECURITY: OTP-KEYWRITER

Part Number: AM263PX-RESTRICTED-SECURITY

Hi Team , 

     as mentioned in otp_keywriter_am263px_SR_10_10_01_00_00  I have followed below steps:
Step1 : started generating keys , keys generation successfully completed . 
Step2 : Certificate generated.

WhatsApp Image 2025-12-10 at 17.21.52.jpeg
Step3 : Inorder to bulid application we run clean command as mentioned and then run make command inorder to generate .tiimage . 

            First time it shown some error , again without cleaning we tried running the same commnad now .tiimage is generated . 
  
            Query : Why there is need of entering command 2 times . 


WhatsApp Image 2025-12-10 at 18.56.13 (1).jpeg
WhatsApp Image 2025-12-10 at 18.56.13.jpeg
Step4: UART MODE : 
           We tried running generated .tiimage in UART mode , we entered command as per the document . After cleaning and running it is now priniting nothing like hash values etc., 
           In general as per the document it will print some commands in dry run mode . 

           Query : What is the issue for not printing anything in dry run mode.

WhatsApp Image 2025-12-10 at 18.52.25.jpeg
           UART MODE with TERA TERM : 

            we have used tera term application inorder to send file as mentioned in the document , video of this attached below . 
 
             Query : After transfering file by selecting XMODEM it is not showing any transfer indication. 


Step 5 : Dev BOOT MODE : Since UART MODE NOT SUCCEDED we tried of running in Dev BOOT MODE.

             we created .ccxml file and then launch configurations done , and then we made changes in the load_sbl.js file as mentioned in the document , now we entered command in scripting console . After running it . it is automatically running the sbl_keywriter firmware . and also it not printing SUCCESS in the console . 

            Query : In console only starting bootloader is printed , and also code started running automatically after doing above steps . when clicked on pause , it is routing to HSM Clients reated .c file.

tidrive.ext.ti.com/.../