Part Number: AM263P4
Hi, I wonder if an external RAM chip could interface the AM263P4 through the OSPI interface, e.g. an Infineon PSRAM with xSPI octal interface and 3V operating voltage could theoretically work?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM263P4
Hi, I wonder if an external RAM chip could interface the AM263P4 through the OSPI interface, e.g. an Infineon PSRAM with xSPI octal interface and 3V operating voltage could theoretically work?
Best regards
Hi Michele,
Yes, you can interface an external PSRAM (such as the Infineon PSRAM with xSPI octal interface) to the AM263P4 through the OSPI interface. However, there are some important hardware considerations to keep in mind:
Key Hardware Considerations:
DQS Line Configuration:
Chip Select (CS) Pin Placement:
Best Regards,
Mayank Shadwani
Hi, Mayank !
Many thanks for your reply!
If I understand correctly:
I see that in the schematics of the AM263P Launchpad the DQS is pulled high:

while in the AM263P technical reference manual spruj55d, it is suggested to use a pull down on it:
13.3.2.2.5.4.2.1.4 External Pull Down on DQS
Per the OSPI protocol, the FLASH device drives DQS while CS is asserted. When CS is not asserted the FLASH
device presents HiZ on DQS. When configured to use DQS, the controller uses the DQS as a clock, which
samples the incoming data into a FIFO. Noise on the DQS when it is HiZ can cause spurious false triggering of
the FIFO and filling it with invalid data. There is no way to clear this data except to reset the OSPI module.
To avoid this issue, it is recommended to add a pull down on the DQS line.
¿So I wonder if
Many thanks again
Michele
Hi Michele,
Thank you for your detailed questions regarding the DQS signal configuration. Let me address each of your points:
Yes, your understanding of the DQS functionality is accurate:
You correctly observed that the AM263P LaunchPad uses a pull-up configuration, which differs from the Technical Reference Manual recommendation. The pull-up configuration on the LaunchPad was intentionally implemented to provide hardware with all possible configurations for evaluation and testing purposes. This allows developers to test different scenarios during the development phase.
However, for the AM263P Control Card, we use a pull-down configuration, and everything works fine with that setup as well, which aligns with the TRM recommendation.
a pull down on DQS could work OK too in a board where both a PSRAM and an OSPI chip are connected to the TI OSPI interface (with different CSs)
The AM263P LaunchPad does not have provisions for connecting both Flash and PSRAM simultaneously using two separate chip selects. The board features a single OSPI memory slot that supports either a Flash or a PSRAM device at one time.
For custom board designs where you plan to connect both Flash and PSRAM to the OSPI interface using different chip selects, a pull-down resistor on DQS will work correctly for both device types. However, please note the following important consideration:
Please let me know if you need any further clarification or have additional questions.
Best regards,
Mayank Shadwani