Part Number: MSPM0L1105
Other Parts Discussed in Thread: SYSCONFIG
Hi TI experts,
I want to use the SPI function of my MSPM0L1105 device in peripheral mode.
So, the CS pin of the should be an input. But when I check it with the probe of my oscillocsope, it goes to GND. I have a pull-up on this pin (10k) and the voltage falls to 2.4V (the supply is 3.3V).
I have tested to set 3 wires-mode, 4 wires mode, ti-asynchronus mode, with and without pull-up, but it don't works.
I'm sure that it is not a hardware issue on my boars because when I disble the SPI module and set the pin as a GPIO input, the voltage goes to 3.3V....
Any idea ?
thanks for your reply.
BR