Part Number: AM2634
- Is it mandatory to flash the HSM Runtime image when operating in HS-SE mode?
- Is it also required that the HSM Runtime image gets loaded into the HSM core (includes certification verification and image integrity validation) regardless if we are using any of its services in the SBL.
- Do the HSM Runtime Firmware and the SBL image share the same memory regions in QSPI flash memory ( 0x0_0000 - 0xF_0000 and 0xF_0000 - 0xX_0000 (start of app image) )?