Part Number: MSPM0G3507
Hi there,
We are using the MSPM0G3507 LaunchPad and testing the BIM demo
(path: ti/mspm0_sdk_2_08_00_03/examples/nortos/LP_MSPM0G3507/boot_manager/boot_application).
We have a couple of questions regarding firmware updates:
Rollback Support: If a firmware update fails or is interrupted, does the BIM demo support rolling back to the previous firmware?
Custom Implementation: If rollback is not currently supported, is it possible to modify the code to implement this functionality? If so, could you provide recommend on which parts of the code should be adapted?
Thank you for your help:)
Best regards,
Ziqiang