This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Selection of External 4MHz to 48MHz crystal oscillator (HFXT) on MSPM0G3507

Part Number: MSPM0G3507

Hi 

The documents for MSPM0 G-Series 80MHz Microcontrollers and MSPM0G350x Mixed-Signal Microcontrollers with CAN-FD Interface do not mention the selection of an External 4MHz to 48MHz crystal oscillator (HFXT).

The MSPM0G3507 EVM uses a 40MHz 12.5pF crystal.

Our original MSPM05117 board used a TXC/7M40000183 XTAL 40MHz 15pF/10PPM , and the datasheet is  attached TXC_7M40000183.pdf .

Is the MSPM0G3507 suitable for use with the TXC/7M40000183?

Please provide the specifications for External crystal oscillator (HFXT) to us, thanks.