Part Number: MSPM0C1104
Dear Sir,
Please help regarding following concerns for the code hysteresis loop for sensor (ADC).
following code is woking perfectly on the launch pad.But same code when dumped on the 8 pin MCU on the application board found some times working some times not working.
Also delay_cycles (100) is not giving same delay every time.
#include "ti_msp_dl_config.h"
volatile bool gCheckADC;
volatile uint16_t gAdcResult;
volatile int16_t gADCOffset;
bool LED = false;
volatile uint16_t gCounterutp;
volatile uint16_t gCounterltp;
int main(void)
{
delay_cycles(100);
SYSCFG_DL_init();
gCheckADC = false;
gCounterutp = 0;
gCounterltp = 0;
DL_GPIO_setPins(GPIO_GRP_0_PORT, GPIO_GRP_0_PIN_0_PIN);
gCounterltp = 0;
/* Get calibrated ADC offset - workaround for ADC_ERR_09 */
gADCOffset =
DL_ADC12_getADCOffsetCalibration(ADC12_0_ADCMEM_0_REF_VOLTAGE_V);
NVIC_EnableIRQ(ADC12_0_INST_INT_IRQN);
while (1)
{
DL_ADC12_startConversion(ADC12_0_INST);
while (false == gCheckADC) {
__WFE();
}
gAdcResult = DL_ADC12_getMemResult(ADC12_0_INST, DL_ADC12_MEM_IDX_0);
if (gAdcResult < 0x1E) //96mv //30 ADC value
{
if (gCounterutp == 0x03) {
DL_GPIO_clearPins(GPIO_GRP_0_PORT, GPIO_GRP_0_PIN_0_PIN); // LAMP on
DL_GPIO_clearPins(GPIO_GRP_0_PORT, GPIO_GRP_0_PIN_0_PIN); // LAMP on
gCounterutp = 0;
} else {
delay_cycles(12000000 * 8); // 12000000 //1505000 // 2sec dealay
gCounterltp = 0;
gCounterutp++;
}
gCheckADC = false;
DL_ADC12_enableConversions(ADC12_0_INST);
}
else {
if (gAdcResult > 0xE6) // 25//37D//740mv 230 adc value
{
if (gCounterltp == 0x03) {
DL_GPIO_setPins(GPIO_GRP_0_PORT, GPIO_GRP_0_PIN_0_PIN);
DL_GPIO_setPins(GPIO_GRP_0_PORT, GPIO_GRP_0_PIN_0_PIN);
gCounterltp = 0;
} else {
delay_cycles(12000000 * 8); // 12000000 //1505000
gCounterutp = 0;
gCounterltp++;
}
gCheckADC = false;
DL_ADC12_enableConversions(ADC12_0_INST);
}
}
}
}
void ADC12_0_INST_IRQHandler(void) {
switch (DL_ADC12_getPendingInterrupt(ADC12_0_INST)) {
case DL_ADC12_IIDX_MEM0_RESULT_LOADED:
gCheckADC = true;
break;
default:
break;
}
}