Is this the status of CortexR4F MPU or something else?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Eugene,
We have received your post and have forwarded to one of our experts.
SYSESR.MPMODE was originally defined to support a feature on the ARM 10 class CPUs that were an original target of the platform architecture. ARM 10 has the capability to implement MPU or MMU, which would be indicated via this status bit. As no ARM 10 devices were produced, the bit is effectively a don't care.
Regards,
Karl