Part Number: MSPM0G3107
Other Parts Discussed in Thread: SYSCONFIG
hi,
Based on the mspm0_sdk_2_08_00_04 sdk, the 32pin package of MSPM0G3107 is provided. Since there is no sample corresponding to 3107 in your sdk, please provide a bare-metal driver for the spi and uart2 of the 3107 spi0 three-wire.
1.The pin definitions of the spi0 driver: CLOCK: PA11, PICO: PA9, POCI: PA10, CS: PA8(general gpio). bit rate:4M, Clock Polarity :High, Phase :Data captured on first clock edge, Mode Select :Control
2. Pin definitions of Uart2, TX: PA21, RX: PA22