This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4: Verification of Keyring keys inside HSM Secure RAM

Part Number: AM263P4
Other Parts Discussed in Thread: SYSCONFIG

Hi,

Im using AM263P4 LP with 

mcu_plus_sdk_11_00_00_19

tifs_am263px_11_00_00_01

sysconfig 1.25

ti_arm_clang compiler 4.0.3 with CCS version 20.30(recommended)

I have changed the board name to HS in devconfig.mak file

I tried to verify the process of keyring and importing in SBL_null(LP) in HS-FS device.

I have followed the procedure (refer hyperlink )to verify the imported keys in Secure RAM after loading of SBL_null.

Integration in Secondary Boot Loader (SBL) 

Im struck in the Step 5. In UART mode, I used Tera term application to send the default_sbl_null.cfg file into the flash as per given the above source. But the loading is not successful, the transfer doesnt happen and struck at some point(everytime % transfer is same).

Although I use python script(provied in the source), i dont get printed anything on the console.

How can I solve this issue?

 

Also I am not able to import the hsm firmware from tifs_am263px_11_00_00_01 in CCS 20.30, it says compatible version is not installed. The above versions remain same. What can I do here?

Thanks and Regards

Geetha K