Part Number: AM2634-Q1
Other Parts Discussed in Thread: MCU-PLUS-SDK-AM263X, SYSCONFIG
Hi,
For our application, the device has to get IP address using dhcp with hostname. For making this work, I have set the options below to 1.
File-->C:\ti\mcu_plus_sdk_am263x_10_02_00_13\source\networking\lwip\lwip-stack\src\include\lwip\opt.h
#define LWIP_DHCP_DISCOVER_ADD_HOSTNAME 1
#define LWIP_NETIF_HOSTNAME 1
in my application, I set the hostname with the below line.
Open MAC port 1
EnetPhy_bindDriver:1873
Open MAC port 2
EnetPhy_bindDriver:1873
PHY 3 is alive
PHY 12 is alive
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 70:ff:76:1f:db:4e
Host MAC address-0 : 70:ff:76:1f:db:4f
Enet IF DOWN Event
Cpsw_handleLinkUp:1653
MAC Port 1: link up
Network Link DOWN Event