This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: MSPM0C1104: BSL Serial Port Programming Failure

Part Number: MSPM0C1104

## Problem
BSL_GUI_EXE fails to program MSPM0C1104 via serial port with two errors:

1. **Mass Erase (0x15)**: Returns `BSL:00` instead of `00 08 02 00 3B 00 38 02 94 82`
2. **Program Data (0x20)**: No response (timeout)

Serial port sniffer data is attached for analysis. 

## Environment
- **Hardware**: LP-MSPM0C1104
- **OS**: Ubuntu 22.04
- **SDK**: MSPM0 SDK 2.08.00.03 (installed via CCS 20.3.1.00005)
- **BSL**: flash_bsl
- **Application**: bsl_software_invoke_app_demo_uart

## Request
Can you confirm if BSL_GUI_EXE serial programming is supported on LP-MSPM0C1104?
We need verification that this workflow should work before investigating further.