This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1507: MSPM0G1507 program for help

Part Number: MSPM0G1507
Other Parts Discussed in Thread: UNIFLASH

Hello
I have a little difficulty using the XDS110 (official) burner to MSPM0G1507 program:
Burning environment: CCS12.3, XDS110, uniflash
Programming wiring: 0.1uf capacitor in series between VSS-GND, VDD-VREF, SWDIO-SWDIO, SWCLK-TCK, VSS-VDD, and external 3.3V to VREF and GND
Programming process: CCS is compiled and burned directly
Error message: CS_DAP_0: Error connecting to the target: (Error -267 @ 0x0) The controller could not detect valid target supply. Check target JTAG connection and/or connection setting specifying voltage level. (Emulation package 9.11.0.00128) 
The reason for querying the error information is that the target board is not powered on, but it has been absolutely confirmed that there is no problem with power
Please help me see why