Part Number: AM261-SOM-EVM
Other Parts Discussed in Thread: LP-AM261
Hi all,
I got a LP-AM261 to run sdk-am261x_11 examples with ccs 20.4, connect with uart(J24) and power(J25)
ex. gpio_led_blink_am261x-lp
I let the while(true) loop to keep running, made a counter(global variable) and keep LED blink, start run is good but it will no active after few seconds or minutes with no reason. The threads state shows cortex_R50 is still normal running but LED no more active, pause and continue has no response. How can I solve it and what's wrong?
Same project, a variable add to watch expression and continuous refresh, but it's not work when programe is running. Use breakpoints I can shure the variable has change. How to solve it to check the variable in real-time when programe is running?