This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0G3519: XDS110 Not Recognized in CCS Theia (LP‑MSPM0G3519)

Genius 3215 points

Part Number: LP-MSPM0G3519
Other Parts Discussed in Thread: MSPM0G3519, TMDSEMU110-U

Hi All,

I’m currently trying to connect the XDS110 to the LP‑MSPM0G3519, but CCS Theia cannot detect the XDS110 and I can’t establish a connection.

  • 3.3 V is supplied from J5 (directly to the LP‑MSPM0G3519).
  • The jumpers are configured to isolate/disconnect the MSP432 (on‑board XDS110) on the evaluation board.
  • I confirmed on the PC that the XDS110 is recognized over USB.
  • Without using the XDS110, I was able to confirm a connection to the LP‑MSPM0G3519 alone.

image.png

image.png

image.png

image.png

Best Regards,

Ito