Part Number: MSPM0L2228
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Hi,
I'm trying to use a sample software of TI for MSPM0L2228 "secondary_bsl_uart"
But the following error was shown and can't start the software.
Could you tell me how to resolve this issue???
1) Execute CCS
2) "Get Started Screen" is shown
3) Click "Browse software and examples"
4) Import "secondary_bsl_uart" from "Arm-based microcontrollers/Embedded Software/..."
5) Select "MSPM0L2228" for Target device
6) Click "NEXT" button
7) Re-build from the menu "Project/Rebuild Projects"
8) The following 2 warning are shown
[10]warning: /ti/project_config/ProjectConfig: Project Configuration File generation is disabled for this project. SysConfig Project Migration is not currently supported for this project.
[11]warning: /ti/driverlib/NONMAIN staticWriteProtectionNonMain: This locks the configuration permanently unless BCR factory reset is enabled with or without password.
[43]warning #10247-D: creating output section ".binit" without a SECTIONS specification
9) Connect the Lauchpad with USB cable to PC
10) LED2 on the Lauchpad turn on to Green
11) Click "Debug Project" from "EXPLORER" pain on the left side of CCS
12) The following messages are shown on the "Debug output" area and the sample software was not loaded to the launchpad.
Flash Programmer: Device does not contain data bank
File Loader: Memory write failed: Flash Programmer: MAIN/NONMAIN/DATA erase failed!
GEL: File: C:\Users\backend-soft01\workspace_ccstheia\secondary_bsl_uart\Debug\secondary_bsl_uart.out: Load failed.