This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: DMA write GPIO failure

Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG

Hello,

When I try to write GPIO via DMA, after official init SYSCONFIG_WEAK void SYSCFG_DL_DMA_init() I have also:

    DL_GPIO_enableDMAAccess(GPIOA, DL_GPIO_PIN_3);     
    DL_DMA_setSrcAddr(DMA, DMA_CH0_CHAN_ID, (uint32_t)&gPA3_CLR);
    DL_DMA_setDestAddr(DMA, DMA_CH0_CHAN_ID, (uint32_t)&GPIOA->DOUTCLR31_0);

In advanced it has been confirmed that DMA0 work correctly for data transfer by replaced src/dest address with pre-set fixed addr. to fixed addr. at least the DMA trigger happened and static src data(0x12345678) been transfered to dest(printout to check) successfully, just not sure the DMA 'repeat single' setting correct or not cause static data used to verify the data transfer, maybe it just transfer for only once.  should i use fill data extend mode or block to block mode, or any other more missed please help.

Thanks