This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: CRC15 Usage

Part Number: TMS570LC4357

Hello ,

I use canbus protocol for communication. But should i setting crc during data transmit or receive. If i should setting , how can i do ? if i dont setting crc15 ,  does tms device do it ?

  • Hi Dobby,

    You do not need to use CRC module for CAN communication. CAN Hardware automatically generates and checks the CRC field during transmit and receive.

    The CAN protocol itself defines the CRC field (CRC-15 for classical CAN). The CAN controller automatically calculates CRC and appends it to the frame on transmitter side, and on receiver end CAN controller automatically checks the CRC.

    If CRC is wrong the frame is rejected and an error frame is generated.

    --
    Thanks & regards,
    Jagadish.