Part Number: TIDM-02010
Hi,
We are working on TIDM-02010 model. Here at output of microcontroller, we are getting PWM's (with glitches), at output when there is no load we are able to change the frequency of PWM duty cycle to 80Hz(Max we have checked). But, when the compressor motor is connected we are not able to run compressor more than 25Hz PWM Duty cycle. When we are increasing the Frequency of varying the Duty cycle more than 25Hz, it is generating the fault at IPM. The Bootstrap capacitors we will be using are 10uF/63 Electrolytic capacitor and 0.1uf Ceremic capacitor. I have not mounted the Bootsrap diode as datasheet mentioned that it has inbuilt bootrap diode. Help me if i am making any mistake.What could be the problem i am making in it.