AM263P4: Register Addendum contains incorrect EPWM registers

Part Number: AM263P4


I am reading the register addendum, document SPRUJ57B with a may 2025 revision, and noticing that the EPWM registers are all incorrect. In section 3.8.1, table 3-569, all of the instances are listed and the addresses are correct.  Just below that at table 3-570 are the EPWM Registers, which is almost entirely incorrect. In table 3-570, only EPWM00_G0 is correct.

If you compare the base address of EPWM01_G0 from table 3-569 it is listed as 0x50001000. If you look at the base address of EPWM01_G0 in table 3-570, it is 0x50040000 which is incorrect. Please fix this.