This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1105: How to use linker file definitions.

Part Number: MSPM0C1105

#define FLASH_STARTING_ADDRESS   0x00000000U

 

Can we use the definitons from the linker file rather than hardcoding address here

  • Hi Santhosh,

    Can you provide more context to this? I am not sure I quite understand what you are asking. Do you mean if you can use definitions as the values inside of the memory directive?

    MEMORY
    {
        FLASH           (RX)  : origin = 0x00000000, length = 0x0000FFF8
        SRAM            (RWX) : origin = 0x20000000, length = 0x00001000
        BCR_CONFIG      (R)   : origin = 0x41C00000, length = 0x000000FF
        BSL_CONFIG      (R)   : origin = 0x41C00100, length = 0x00000080
    }

    Best,

    Owen

  • /* Start of flash memory region */
    #define FLASH_STARTING_ADDRESS                     0x00000000U

    /* End of flash memory region */
    #define FLASH_ENDING_ADDRESS                       0x00007FFFU
    Instead of hardcoding the address, are the definitions provided in the linker file. So that i can use in .c files 
  • Hi Santhosh,

    There aren't definitions generated for the origin and length in the linker file that you can use in C files. Hardcoding these definitions is likely the best option since memory layouts rarely change during development and it requires the least amount of changes to your project.

    If you want to create definitions within the linker file, you would still have to hardcode them. Furthermore, you would have to disable linker file generation within the .syscfg file so that these definitions don't get erased upon building the project. I personally wouldn't recommend this. However, if you want to follow this approach, this is an example of what you would need to add to your linker file:

    __FLASH_START = 0x00000000;
    __FLASH_END   = 0x0000FFF7;    /* 0x00000000 + 0x0000FFF8 - 1 */
    __FLASH_SIZE  = 0x0000FFF8;
    __SRAM_START  = 0x20000000;
    __SRAM_END    = 0x20000FFF;    /* 0x20000000 + 0x00001000 - 1 */
    __SRAM_SIZE   = 0x00001000;

    You would need to make a copy of the linker file and move it outside of the Debug folder.

    Upon building, you can observe GLOBAL SYMBOLS in the .map file. You can then access them in your C file like so:

    extern const uint32_t __FLASH_START;
    extern const uint32_t __FLASH_END;
    extern const uint32_t __FLASH_SIZE;
    extern const uint32_t __SRAM_START;
    extern const uint32_t __SRAM_END;
    extern const uint32_t __SRAM_SIZE;
    
    #define FLASH_STARTING_ADDRESS  ((uint32_t)&__FLASH_START)  // 0x00000000
    #define FLASH_ENDING_ADDRESS    ((uint32_t)&__FLASH_END)    // 0x0000FFF7

    As you can see, this is much more work than hardcoding the definitions in your .c or .h file. 

    Best,

    Owen

  • Thank you for the reply

    How to access this variable without using global variable which means without extern.

    I know static declaration it won't work. Any other idea directly access from the Linker file without using global variable.

  • Hi Santhosh,

    I understand the confusion about 'global variables,' but linker symbols are fundamentally different from regular global variables.

    The extern declarations are not creating global variables. They're telling the compiler how to access symbols that the linker creates. This is the standard, industry-accepted method used in all embedded systems.

    There is no other way to access linker-defined memory regions in C code.

    Is there a reason why you don't want to hardcode definitions? This would be essentially as maintainable as defining symbols in the linker file.

    Best,

    Owen