Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: EnDat Propagation Delay depends on PRU Clock

Part Number: AM2434

Hi experts,

i found the following strange behaviour concerning the EnDat Propagation Delay Measurement.

  • Motor Control SDK 11.00.00.06
  • EnDat Diagnostic Example, multichannel (0+2), loadshare

In the example, the PRU core clock is set to 200Mhz. Then i get the following propagation delay measurements from the EnDat PRU firmware:

  • Channel0: 95ns
  • Channel2: 115ns

When i change the PRU core clock to 300Mhz, the measurements change:

  • Channel0: 115ns
  • Channel2: 130ns

Is this behaviour expected?

Best Regards,
Stefan Schlee