This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: System Configuration Setup

Part Number: MSPM0C1104
Other Parts Discussed in Thread: UNIFLASH

Hello!

Trying to use the MSPM0C1104 in 8pin SOT to provide some PWM-generated clocks...

Have some questions about that:

  1. Are you going to implement fully functioning  SYSCTL in Zero Code Studio? It is possible to configure HFCLK and CLK_OUT pins in ZCS project, but not the internal clock tree, not possible to use the pins in such modes...
  2. I moved to CCS (Win11), was able to configure the HFCLK pin on the default reset pin. It works and the output signals' jitter became significantly lower as well as I am using an external 24MHz oscillator. My question is - will the MCU starts properly if I have a 24MHz clock on a default reset pin on power-up? How, in general, to use all 6 awailable pins and have an ICP functionality?
  3. I was not able to flash the MCU from CCS. I have to open the out file with UniFlash. I have a valid ccxml file and can test dongle and MCU connections. How to enable the flashing from CCS?


Regards,

Konstantin