Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Hi Champs:
My cust reported a very strange problem:
The situation is like this:
CaseA: CCS12.7.0 + Sysconfig 19.x + Complier LTS 4.1
CaseB: CCS12.8.1 + Sysconfig 20.x + Complier LTS 4.2
The build-out .Out/.Hex file are not the same between CaseA and Case B.
Even they are using the same C project code.
Do you ever see this kind of issue?
BR Rio