This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: Programming failure

Part Number: MSPM0C1104

my customer is using MSPM0C1104 and  they are using SWDIO multiplexing for GPIO INPUT function, after the program burn in, can no longer perform debugging and programming. do u have any advise on this? thanks!

  • Hi Zoey,

    If the SWDIO pin is re-purposed in application code, you can issue a factory reset to be able to re-program the device.

    Section 7.1 in the MSPM0 MCUs Development Guide outlines how to factory reset a device. I would recommend using the Factory Reset Manual option.

    Debugging will not be possible if the application sets the SWDIO pin to have GPIO functionality during runtime.

    Best,

    Owen