This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507-Q1: Is Rosc 100kohm with 0.1% accuracy required?

Part Number: MSPM0G3507-Q1

Hello Team,

According the MSPM0 datasheet, Rosc 100k ohm (0.1%) is recommended for SYSOSC FCL feature. 

Customer is using LIN at 19200bps with target accuracy ±1.5% as well as SPI communication.

Would it be mandatory to use FCL feature in this case and add external 100k (0.1%)?

Or is it okay to use 100k (1%) instead?

Thank you for your support!

Best regards, 

Robin Kim