This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263PX-MCAL-SDK: AM263PX HSM_CLIENT Call Issue

Part Number: AM263PX-MCAL-SDK

I am running SDK version 11_00_00_19 and TIFS version 11_00_00_01 and have flashed my keys to my board and converted it to HS_SE mode and can validate that the hashes of the keys on the board are what is expected. 

I have been able to flash and run multiple different applications - all of the AES provided examples from the SDK in addition an application I wrote seperatly. 

A few weeks ago I was working on an AM263P board and was able to write and execute code that called upon the proc_auth_boot hsm client to validate an image and it executed correctly. I just started over with a new AM263PX board and have been able to execute everything but any HSM_Client Calls. 

Calling proc_auth_boot (HsmClient_procAuthBoot) fails with the  [HSM_CLIENT] Proc_Auth_Boot request NACKed by HSM server error but I can validate that is is reading the certificate and image in flash correctly before that call is made. 

Also running an SBL that disables the HSM debug firewall with the certificate generated for my board returns this error:

[HSM_CLIENT] OpenDbgFirewall request NACKed by HSM server

Starting OSPI Bootloader ... 
SBL failed!!

 In addition - running the hsm_services example executed correctly without any issues.

Is there anything I should look into specifically to resolve this problem or is there something I am overlooking?

  • Update: through tracing I found it is failing at line 1467 of tifs_am263px_11_00_00_01\source\modules\cert_auth\asn1_parse.c

    For more insight on when this is being called here is the path traced out:

    ASN1p_end (the function failing) is being called by  ASN1P_public_key_info ~called by~ ASN1P_tbs_certificate ~called by~ ASN1P_parseX509Cert ~called by~ Cert_Auth_validateCertAgainstKey ~called by~ SEC_DBG_handleOpenDebugReq

    Does anyone have any insight at what this means in wrong? The certificate that it is validating is created using my root of trust private key. 

  • Hi Addison,

    I just started over with a new AM263PX board and have been able to execute everything but any HSM_Client Calls. 

    On the new board, can you confirm if your device is in HS-SE state with the same keys as the previous board?

    The parsing typically fails if the ROT keys mismatch. 

    Thanks and Regards,

    Nikhil Dasan

  • I confirmed it is in HS-SE with the same keys

  • Hi Addison,

    Sorry for the delayed response.

    running the hsm_services example executed correctly without any issues.

    You mentioned that the hsm services are working on this board.

    For eg. You are able to run the getversion() service from an example but not from your application. Is that correct?

    If yes, Could you let me know the below?

    1. Are you using the same bootloader in both cases to load these application?

    2. Are you using the same HSMRT firmware to load these 2 applications?

    Thanks and Regards,

    Nikhil Dasan