Part Number: MSPM0L1227
Other Parts Discussed in Thread: SYSCONFIG, LP-MSPM0L2228,
Hi,
My customer has a question about the specification of Flash Memory Stack Write Protection (SWP).
According to the TRM, it seems that the first 32Kbyte can be set as SWP by one sector, and the other can be set by eight sectors.
They wanted to use this function to disable SWP only for certain sectors of Flash Memory on Sysconfig in CCS and enable other regions in order to internally rewrite in the SWP disabled area even after writing ROM.
However, this operation failed to write the SWP disabled area, and the operation did not work as intended.
Could you please let them know if there is a wrong recognition or usage of this feature.
From the description of SWP Register in TRM


The Screen of SysConfig
Sysconfig>Software>Configuration NVM>SWP Configuration CCS

They set the sector 0 to 3 : bit[3:0] in the first 32Kbyte as “1” (Disabling protection), and the sector 4 to 31 : bit[31:4] are set as “0” (Enabling Protection).
Thanks and regards,
Hideaki