Part Number: MSPM0G3519
Hi TI Team,
Currently I'm working on ADC topic with external voltage reference in my project. I have one question that I'm using 3.6V as external voltage reference for ADC , and I select external ref as configuration, with ADC 10 bit resolution => I understand that the ADC will scale with Vref = 3.6 V, right ? (3.6V is equivalent to 1023). Is the configuration of BUFCONFIG in CTL0 affects to this value ? Because I saw that there is only 2 options 1.4V and 2.5V. I don't know how this will affecto the result.