Part Number: MSPM0-SDK
Other Parts Discussed in Thread: SYSCONFIG, MSPM0G3507
Dear TI Support Team,
I am reporting what appears to be a bug-like behavior in the SysConfig tool for the MSPM0 SDK. I would appreciate your guidance on the phenomenon and any recommended countermeasures.
Phenomenon:
When configuring SysConfig based on the sample code (mspm0_sdk_2_09_00_01\examples\nortos\LP_MSPM0G3507\driverlib\adc12_single_conversion_vref_internal) as attached, the GPIO settings are not included in the output files (ti_msp_dl_config.h), resulting in errors.
VREF_INTERNAL_POS_NEG.txt 

My Situation:
In the product I am developing, VREF is used in Internal mode, and to reduce power consumption, I need to switch VREF ON and OFF as needed. Without GPIO definitions, I cannot control this, which is critical for my application.
Could you please explain the cause of this phenomenon and suggest countermeasures? For example, is there a way to manually add GPIO settings or modify SysConfig to ensure they are generated for Internal mode?
Thank you for your assistance. I can provide additional details, such as the attached .syscfg file or error logs, if needed.
Best regards,
Tsuchiya.