Part Number: AM2434
Hello,
during "Interoperability IRT legacy" testing with the AM243x‑EVM based device (DUT), we observe that all devices connected downstream of the DUT intermittently lose connection.
Wireshark shows repeated AR consumer DHT/WDT expired (RTA_ERR_ABORT) events at frames 43268, 43336, 43708, 43738, 43902, 44195, 44218.
The issue appears only when traffic passes through the DUT; direct connections do not show watchdog expirations.
Special old PLC (S7-300 CPU319F-3 PN/DP) supporting "Legacy IRT" communication required for this test scenario (because no issue in "Advanced IRT" communication).
Using industrial SDK v 11.00.00.13, the same behavior also with the pure "AM243x‑EVM" device (devkit)!
Could you please advise:
1) Why might the AM243x‑EVM delay or drop PROFINET IRT frames, causing DHT watchdog triggers?
2) Are there known limitations or required settings for stable IRT‑legacy operation on AM243x (PRU‑ICSS timing, CPSW queues, sync settings, reduction ratio, send‑clock)?
3) And mainly, how to fix it?
Wireshark capture attached.
Best regards,
Vit Triska
tc-interoperability_IRT-legacy.zip