Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: Powering up on HFCLK

Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG

Hi there,

I have MSPM0G3507 Launchpad here. First steps: I am migrating from MSP432 which was an amazing MCU. 

I managed to get it to receive UART packets where UART is being clocked by SYSPLL. Now I want to switch to the external crystal clock which is 40MHz. On the surface there shouldn't be a problem: in syscgf I am configuring:

MCLK sourced from HSCLK

HSCLK sourced from HFCLK

Enable HFCLK: ticked

HFCLK Source : HF External XTAL

Set External HF Clock Frequency (Hz) : 40 000 000

External HF Clock Frequency: 40.00MHz

The above configuration completely bricks the Launchpad when attempting to debug. It does behave as if I have forgotten to enable the external clock. 

There is an example of using external clock but MCU there boots on SYSCLK after which the swich is made to HFCLK through code.

Can the board boot directly in HFCLK?

Cheers

Dimo