TM4C1233H6PM: TI Driver Question

Part Number: TM4C1233H6PM

Hi Team,

We are developing code for TI TM4C1233H6PM microcontroller. We have TI rtos and also TI boot code from TI.

In TI code bl_can.c file, there is a function called CANMessageGetRx() inside it where have code like this:

    if ((ui16MsgCtrl & (uint16_t) (CAN_IF1MCTL_NEWDAT | CAN_IF1MCTL_MSGLST))

            == (uint16_t) CAN_IF1MCTL_NEWDAT)

    {

        //

        // Get the amount of data needed to be read.

        //

        ui32Bytes = ui16MsgCtrl & (uint16_t) CAN_IF1MCTL_DLC_M;

 

        //

        // Read out the data from the CAN registers 16 bits at a time.

        //

        pui16Data = (uint16_t*) pui8Data;

 

        pui16Data[0u] = CANRegRead(CAN0_BASE + CAN_O_IF1DA1);

        pui16Data[1u] = CANRegRead(CAN0_BASE + CAN_O_IF1DA2);

        pui16Data[2u] = CANRegRead(CAN0_BASE + CAN_O_IF1DB1);

        pui16Data[3u] = CANRegRead(CAN0_BASE + CAN_O_IF1DB2);

 

        //

        // Now clear out the new data flag.

        //

        CANRegWrite(CAN0_BASE + CAN_O_IF1CMSK, (uint16_t) CAN_IF1CMSK_NEWDAT);

 

        //

        // Transfer the message object to the message object specific by

        // MSG_OBJ_BCAST_RX_ID.

        //

        CANRegWrite(CAN0_BASE + CAN_O_IF1CRQ, (uint16_t) MSG_OBJ_BCAST_RX_ID);

 

        //

        // Wait for busy bit to clear

        //

        while ((CANRegRead(CAN0_BASE + CAN_O_IF1CRQ)

                & (uint16_t) CAN_IF1CRQ_BUSY) != 0u)

        {

        }

    }

    else

    {

        //

        // Data was lost so inform the caller.

        //

        ui32Bytes = 0xffffffffu;

    }

My question to TI is how do we recover from the situation of ui32Bytes = 0xffffffffu?. Any remedy?

To make the code clear to you. I copy the header portion of the code so you can see It is from TI.

//*****************************************************************************

//

// bl_can.c - Functions to transfer data via the CAN port.

//

// Copyright (c) 2008-2020 Texas Instruments Incorporated.  All rights reserved.

// Software License Agreement

//

// Texas Instruments (TI) is supplying this software for use solely and

// exclusively on TI's microcontroller products. The software is owned by

// TI and/or its suppliers, and is protected under applicable copyright

// laws. You may not combine this software with "viral" open-source

// software in order to form a larger program.

//

// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.

// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT

// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR

// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY

// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL

// DAMAGES, FOR ANY REASON WHATSOEVER.

//

// This is part of revision 2.2.0.295 of the Tiva Firmware Development Package.

//

//*****************************************************************************