This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1105: Questions About Entering BSL Mode and UART Command Requirements

Genius 3215 points

Part Number: MSPM0G1105

Hi All,

It was stated that in order to unlock the CPU, it is necessary to connect in BSL mode and then rewrite the device again via SWD.

MSPM0 NONMAIN FLASH Operation Guide 

image.png
I am considering connecting via UART to enter BSL mode, but
what would the UART connection commands be?

Also, is it possible to perform the above procedure using the MSP Gang Programmer,
which has already been discontinued?

Best Regards,

Ito