Part Number: MSPM0G3519
Hi team,
I received a question from an engineer at my customer who is developing with the MSPM0G3519. I have included his question below in blue text:
I’m working on a project trying to validate the MSPM0G3519 for a design. I need to take in a 600 kHz clock and output 6 phase shifted versions of that clock. I’ve been running into issues getting them to output & sync correctly.
I tried to manually configure the device without sys config to use TIMA0 C0 as an input to reset the counter & then output different waveforms with C1-4, but I wasn’t able to get this working correctly. I don’t think that will actually be able to do what I need.
I tried to configure sys config to use a GPIO as an input that triggers an event to TIMA0, & TIMA1, but when I have this running & the same configuration set on the 4 PWM channels on TIMA0 I only get an output on one of them, but the complementary outputs work.
I’m not sure if I’m going about this entirely wrong, but it seems like it should be a relatively simple. I wouldn’t have any trouble doing this with the C2000s I’m used to. Do you have any advice on how to do the 6 phased outputs?
Thank you for the support and please let me know if you have any questions.