This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: MCAN Stuff Error Based on CAN-ID

Part Number: AM6442

Hello, i am having problems with AM64 MCAN module. When sending messages to Can ID's with consecutive zeros stuff error occurs. I am certain that this issue is not related to my hardware because i tested the same bus with different controllers(MCP2518 and Hercules 4357 MCU), i am not having errors. Also this error doesnt occur when there is no receiver for that specific ID. When i changed the CAN ID to value like 0x555555, i didnt have any errors. I thought this might be arbitration issue and i changed the CAN-ID to 0x100000, still had errrors due to consecutive zeros. My Quanta settings are compatible with the other CAN controllers i tested. 

I am using MCAN module in non FDCAN, 1000Kbit, and issue occurs with extended ID's.

What CAN settings should i look into for this issue?