Part Number: MSPM0C1104
I'm using an MSPM0C1104 MCU in the 20 pin QFN package. I'm having it blink a few LEDs in sequence and then make some ADC measurements.
I've had a couple situations where the MCU will look like it locks up. I say look like because it seems to have it's internal clock slow down by about 100x. I'm gauging this based on the LED pulsing with an on-time of 20ms (verified with oscope), which then turned into roughly 2 seconds (also verified on oscope, but as it's rolling mode, is harder to get an accurate measurement).
Unfortunately, it happens unexpectedly and seemingly randomly. It seems to be associated with me touching the PCB, which suggests an ESD event. However, I would expect a latch up or reset to be the result, and not a main clock shift.
Has this been observed in this series?
Are there registers I should be checking the next time this happens? (This assumes that I'll be able to debug it using an SWD debugger)