This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Debugging with AM2434 Cortex-R5 Cores

Part Number: AM2434

Hi,

I'm trying to use the onboard debugger on the AM2434 EVM Board (The Large Green Board), but I'm facing a problem which is the code stucks in the "Udma_open" function. The code stucks in an assert function that returns an error for no obvious reason. And I didn't change anything in it as it is an SDK API. I also recall that this issue faced me with a different peripheral in the "Open" function too.

I want also to mention what I changed. I removed some parts from the generated code regarding the clocks enabling and clock frequency setting. I'm not sure if this the problem or not, I just need assistance to learn if I need that part back as I believe the code is working fine without it.

Thank you in advance.