This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: The ADC NORTOS software routine support

Part Number: MSPM0G3507

Hi,

Please help to provide the MSPM0G3507 software routine for the ADC NORTOS:
There are multiple channels of ADC0, such as ADC0_0~ADC0~3 + power/battery monitor + temperature sensor. Using the DMA method, 16 consecutive automatic samples are taken to obtain 16 sampling values for each channel (or the overall average value is also acceptable).
This driver will be initiated by the application layer once every second. Please inform us of the initialization settings and the calling interface for the driver.
I can't find such an example in TI's mspm0_sdk examples. There are examples for DMA and multi-channel, but I can't find one for both DMA and multi-channel.