This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM33C321A: SPI config

Expert 4736 points

Part Number: MSPM33C321A
Other Parts Discussed in Thread: SYSCONFIG

Hi Champs,

Import Project "spi_controller_command_data_control_LP_MSPM33C321A_nortos_ticlang" from the latest SDK mspm33_sdk_1_02_00_00.

I set MCLK = 160MHz in SysConfig / Clock Tree.

The datasheet says SPI clock can be up to 30MHz. But I can't change the bit rate to a value higher than 16MHz though the SPI Calculated clock source is 80MHz. See the picture below.

MSPM33C321A - SPI clock in SysConfig.png

Please advise if I missed out something or there is something wrong with the SysConfig for MSPM33.

 

Regards,

Kien