Part Number: MSP430FR6043
Hi
can we confirm what the behavior of the USS will be if the DToF calculation window length exceeds the
USS_CAPTURE_DURATION_USEC with the following settings (with water and lobe used):
#define USS_ALG_DTOF_COMPUTATION_MODE USS_ALG_DTOF_COMPUTATION_OPTION_ESTIMATE
#define USS_ALG_DTOF_WINDOWING_MODE USS_ALG_DTOF_EST_WINDOW_OPTION_ESTIMATE
I also have a more general question about the parameters and when they are used:
Could you confirm if:
USS_ALG_WIN_START_INDEX_BACK_OFF_NUM_CYCLES is used with
USS_ALG_DTOF_EST_WINDOW_OPTION_ESTIMATE
And if
USS_ALG_WIN_PEAK_INDEX_2_EDGES_NUM_CYLES is used with
USS_ALG_DTOF_EST_WINDOW_OPTION_DYNAMIC