Part Number: MSPM0L1305
Hi,
I’m using the MSPM0L1305 (16WQFN) and it has BSL_INVOKE multiplexed with an op‑amp input. In my design the pin sits at about 1.4 V during boot because of a resistor divider used for temperature sensing.
1. Is ~1.4 V on the BSL_INVOKE pin during reset safe, meaning it will not trigger BSL mode?
2. If I change the analog input to PA23 (OPA0_IN+) and left BSL_INVOKE pin floating, then will it be ok?
Please note I don't have option to put one more discrete in my board as it is tightly packed
Which is the best solution for this? I dont want my MCU to enter BSL mode always when resets or power cycled