This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4: AM263P4 ECC in RBL

Part Number: AM263P4
Other Parts Discussed in Thread: AM2634

Hi,

I Have some questions regarding TCM and OCSRAM ECC. 

OCSRAM

It seems like the ECC for OCSRAM is enabled by default according to the AM263P4 Register Addendum where ECC Enable, Check and RMW fields have a value of 1 as their reset value. Is this correct? The reason I am confused is because in the following https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1448339/am2634-ecc-on-ocram-ocram-enabled-by-default, It is mentioned that the OCSRAM ECC is not enabled by default for AM2634 which has the same ECC Aggregator register definition as AM263P4.
RBL Initializes OCSRAM banks 0 and 1 completely. Since ECC OCSRAM is enabled by default, all the Error Correcting Code for bank 0 and bank 1 will be set correctly.  What would be the action of RBL when detecting 2-bit OCSRAM ECC error? Does it still pass control to SBL?

TCM

Unlike, OCSRAM, the TCM ECC should be enabled by software. Does RBL code enable the ECC on ATCM and BTCM? 
If the answer is no, what if a 1/2-bit error happens on TCM area that RBL uses? wouldn't that be a safety issue since during RBL execution we can be prone to SEU?

If the answer is yes, What would be the action of RBL when detecting 2-bit TCM ECC error? Does it still pass control to SBL?

Generic

The SDK ECC Code example uses a property for each RAM named "Stride", Does it represents the number of bytes that is used to generate a single Error Correcting Code? 

Thanks,

Pouya

  • Hi Pouya,

    Apologies for the delayed response!

    It seems like the ECC for OCSRAM is enabled by default according to the AM263P4 Register Addendum where ECC Enable, Check and RMW fields have a value of 1 as their reset value. Is this correct?

    You are correct ECC enable and check bits are enabled by default for this device.

    What would be the action of RBL when detecting 2-bit OCSRAM ECC error? Does it still pass control to SBL

    Actually, RBL will not perform any validations related to ECC. But it will do PBIST verifications for L2RAM, TCMA and TCMB. If any actual memory errors in these memories the corresponding PBIST verification will get fail right, if this happens then it will not call the SBL. And then RBL will just stuck in infinite loop without feeding watchdog, so after certain timeout this watchdog will reset the device and again RBL boot process will start again and this process continuous.

    --
    Thanks & regards,
    Jagadish.

  • Hi Jagadish,

    Thank you for your response.

    So RBL won't check for any ECC errors on OCSRAM and won't enable the ECC on TCMA and TCMB. That means while RBL is running if a single bit or double bits flip due to SEU on the TCMA/TCMB memory location used by RBL, or if a double bits flip in OCSRAM memory location used by RBL, then RBL will end up consuming the flipped bits. wouldn't that be a safety issue since the code is using corrupt data? I do not think PBIST can detect an unintended bit flips due to an SEU.

    Thanks,

    Pouya

  • Hi Pouya,

    Apologies for the delayed response!

    Your understanding is totally correct.

    RBL runs PBIST on L2RAM and TCM memories. If PBIST fails RBL doesn't jump to SBL enters an infinite loop and doesn't serve watchdog. Watchdog resets the device and repeats.

    RBL doesn't enable ECC errors for L2RAM and TCM memories.

    Your concern:

    That means while RBL is running if a single bit or double bits flip due to SEU on the TCMA/TCMB memory location used by RBL, or if a double bits flip in OCSRAM memory location used by RBL, then RBL will end up consuming the flipped bits. wouldn't that be a safety issue since the code is using corrupt data

    Yes, theoretically it can.

    However, as per my understanding it is not considered as a safety violation because of below reasons.

    SEU is usually random runtime bit flips. And PBIST is structural test detects stuck-at / coupling / decoder faults. PBIST is not runtime safety mechanism however

    RBL runs very short duration.

    RBL executes before safety functionality is active.

    Doesn't output any safety relevant signals.

    It doesn't have control over safe state and cannot control any output actuators.

    Because of above reasons i am thinking it is not a safety violation.

    --
    Thanks & regards,
    Jagadish.