Part Number: CODECOMPOSER
Other Parts Discussed in Thread: MSPM0G3107, SYSCONFIG
In Code Composer Studio, when creating a new project I am running into trouble with creating a project and in sysconfig there is no PORTB pins. I have a custom board with a MSPM0G3107STI3B8APRQG4 Chip (32 pins). I select none as the board, Device is MSPM0G3107 and the package is VQFN-32(RHB). Nothing I can do will allow me to select either PBx pins or select Port B under Assigned Port. Can someone please tell me what I need to do to be able to use the Port B pins?