Part Number: AM625
Other Parts Discussed in Thread: SYSCONFIG
Hello TI Support Team,
I am currently developing a custom board using the AM6252ATGGHAALWR (AM62x Sitara Processor).
Our system is configured to boot from Standard SPI (MCSPI) — not QSPI or OSPI.
On our design, we have assigned the UART5_RTSN function to pin G25, which is the LBCLKO pin in the AM62x ALW package.
Before fabricating the PCB, we verified this pin-multiplexing configuration using the TI SysConfig tool and also went through a TI schematic review. No warnings were raised regarding the simultaneous use of Standard SPI boot and assigning UART5_RTSN to G25. Based on this, we proceeded with manufacturing our first bring-up boards, and they are currently booting without any issues at room temperature.
However, while preparing for our next board revision, I found a critical warning in TRM Section 5.4.1, which states that for Low-speed SPI boot, the LBCLKO signal must be left unconnected (“absolutely no trace can be connected to LBCLKO”).
This is causing us some concern. If using G25 is strictly prohibited in Standard SPI boot mode, we would be forced to reassign UART RTS to UART0, which is currently dedicated to our internal debug interface — resulting in a noticeable design impact.
Therefore, I would like to request your official guidance on the following points:
Is it absolutely forbidden to use pin G25 (LBCLKO), even if it is muxed to UART5_RTSN, when using Standard SPI Boot?
Does the presence of any physical connection or routing on this pin interfere with the internal loopback circuitry or compromise the Standard SPI boot process in any way?
Any clarification you can provide would be greatly appreciated.
Thank you very much for your time and support.
Best regards,